Adding Components to MQTT FreeRTOS DemoBreaks demo with SDK LWIP Overwrites

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding Components to MQTT FreeRTOS DemoBreaks demo with SDK LWIP Overwrites

537 Views
stevenlutz
Contributor III

I have started with the MQTT FreeRTOS Demo on the MCXN947. The demo works fine, however when a component is added, eg, FlexCan. Then the components get updated including LWIP. 
LWIP is then broken with an error involving the functions for name reoslution. 

In order to move forward and I had to manually copy and include each additional component from another project in order to keep the original LWIP files in place. 

Please advise. Thank you

FRDM-MCXN947 

0 Kudos
Reply
1 Reply

510 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @stevenlutz 

How did you add Flexcan related component?

Will lwip still break when you manually add the relevant code?

BR

Harry

0 Kudos
Reply