MCUXpresso Crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Crash

868 Views
nobodyKnows
Contributor III

Hi,

MCUXpresso crashs sometimes. Mostly if I used "Terminate and Relauch" at debugging.

It seems there is some GTK issue on my Debian 11 OS. The used GTK version is 3.24.24.

 

env SWT_GTK3=0 /usr/local/mcuxpressoide-11.6.1_8255/ide/mcuxpressoide
SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.
Toolbar: com.crt.quickstart.toolbar in menu:com.crt.quickstart.toolbar
Arguments: 

Arguments: 

WARNING: An illegal reflective access operation has occurred
WARNING: Illegal reflective access by org.eclipse.equinox.internal.p2.metadata.expression.Member$DynamicMember (file:/usr/local/mcuxpressoide-11.6.1_8255/ide/plugins/org.eclipse.equinox.p2.metadata_2.6.100.v20210813-0606.jar) to method java.util.Collections$UnmodifiableMap$UnmodifiableEntrySet$UnmodifiableEntry.getValue()
WARNING: Please consider reporting this to the maintainers of org.eclipse.equinox.internal.p2.metadata.expression.Member$DynamicMember
WARNING: Use --illegal-access=warn to enable warnings of further illegal reflective access operations
WARNING: All illegal access operations will be denied in a future release
log4j:WARN No appenders could be found for logger (org.apache.http.client.protocol.RequestAddCookies).
log4j:WARN Please initialize the log4j system properly.
 WARNING: No executable implementation [ExecutableExtensionProvider.getExtensionsMap]

(MCUXpresso IDE:17158): Gtk-WARNING **: 11:19:55.196: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node scrolledwindow, owner GtkScrolledWindow)

(MCUXpresso IDE:17158): Gtk-WARNING **: 11:20:49.949: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node scrolledwindow, owner GtkScrolledWindow)
**
Gtk:ERROR:../../../../gtk/gtktreestore.c:596:gtk_tree_store_get_path: assertion failed: (G_NODE (iter->user_data)->parent != NULL)
Bail out! Gtk:ERROR:../../../../gtk/gtktreestore.c:596:gtk_tree_store_get_path: assertion failed: (G_NODE (iter->user_data)->parent != NULL)
​

 

Is this a known issue? Is there a fix for this?

 

Thanks a lot and best regards,

 

Maximilian

0 Kudos
Reply
2 Replies

845 Views
nobodyKnows
Contributor III

Hi,

good to know but maybe someone knows a solution.

 

Best regards,

 

Maximilian

0 Kudos
Reply

849 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

Unfortunately, the MCUXpresso does not have support for the Debian distro only Ubuntu Linux (64-bit only). 

Best regards,
Pavel

0 Kudos
Reply