build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build error

2,153 次查看
raghu1
Contributor I

fatal error: inttypes.h: No such file or directory
 #include <inttypes.h>

how to find out header file path and how to include.

标签 (1)
0 项奖励
回复
2 回复数

1,944 次查看
BlackNight
NXP Employee
NXP Employee

Could it be that this question is not for MCUXpresso IDE, but for the CodeWarrior and for S08 or S12?

Because the compiler and libraries for S08/S12 are for C89 and they do not include the inttypes.h header file.

Erich

0 项奖励
回复

1,944 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi,

Could you give us more information about the project you are trying to compile and the MCUthat you are using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复