build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

build error

2,147件の閲覧回数
raghu1
Contributor I

fatal error: inttypes.h: No such file or directory
 #include <inttypes.h>

how to find out header file path and how to include.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,938件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Could it be that this question is not for MCUXpresso IDE, but for the CodeWarrior and for S08 or S12?

Because the compiler and libraries for S08/S12 are for C89 and they do not include the inttypes.h header file.

Erich

0 件の賞賛
返信

1,938件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi,

Could you give us more information about the project you are trying to compile and the MCUthat you are using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信