USB CCID Class - Interface configuring

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CCID Class - Interface configuring

2,370件の閲覧回数
sachin_singh
Contributor II

Hi,

I am using PNEV7462C card reader and need to add two interface in CCID class(which can be seen under device manager with SMART_CARD_READERs CLASS with Two interface).

In "phExCcid" example, it shows only single "interface" in SMART_CARD_READERs class. And I need to add one more interface into it.

So, How can I made changes into the Use usb descriptor files to add one more "interface in same SMART_CARD_READERs class.

Looking forward for the response for adding one more "interface" in SMART_CARD_READERs CCID USB Class.

Your all the support and response are highly appreciative.

Thanks in advance

ラベル(1)
0 件の賞賛
返信
0 返答(返信)