Kinetisモータ・スイート

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Motor Suite

838件の閲覧回数
LArmstrong1985
Contributor III

Hi,

I've seen that in the past there is a tool (Kinetis Motor Suite) to design a motor control system

but I don't find it yet on NXP site.

Where I can find it? 

Is there something similar integrated with Mcuxpresso?

Is there any updated documentation to start with a new project in McuXpresso?

Thank you in advance.

0 件の賞賛
返信
1 返信

773件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Fabio,

The Kinetis Motor Suite is an out-dated software, at the moment what we recommend is to use FreeMASTER. FreeMaster is a run time debugging tool that allows the user to create GUIs to fit their needs for their application, such as implement graphs, motor  control, etc.

For the KV31F for example, you can find examples in the SDK for motor control that are FreeMASTER projects.

You can run these examples to see how these complement each other and can help you customize your application.

The exmaples in the SDK for motor control with FreeMASTER are called:

mc_bldc & mc_pmsm

Best Regards,

Sabina

0 件の賞賛
返信