USB CCID Class - Interface configuring

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB CCID Class - Interface configuring

2,365 Views
sachin_singh
Contributor II

Hi,

I am using PNEV7462C card reader and need to add two interface in CCID class(which can be seen under device manager with SMART_CARD_READERs CLASS with Two interface).

In "phExCcid" example, it shows only single "interface" in SMART_CARD_READERs class. And I need to add one more interface into it.

So, How can I made changes into the Use usb descriptor files to add one more "interface in same SMART_CARD_READERs class.

Looking forward for the response for adding one more "interface" in SMART_CARD_READERs CCID USB Class.

Your all the support and response are highly appreciative.

Thanks in advance

Labels (1)
0 Kudos
Reply
0 Replies