ULinkPro MCUXpress

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ULinkPro MCUXpress

3,129 Views
naasikhendricks
Contributor II

Hi I would like to use my UlinkPro to do tracing with Mcuxpress. It is a Eclipse based toolchain and i don't want to mess around too much with current xpress settings.

Kind regards

0 Kudos
Reply
4 Replies

2,947 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Naasik,

It's not sure. You can try. If the ulinkpro firmware is CMSIS DAP, MCUXpresso can support it. You may ask ARM for help.

Regards,

Jig

0 Kudos
Reply

2,947 Views
naasikhendricks
Contributor II
0 Kudos
Reply

2,947 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Naasik,

Ulink2 has a CMSIS-DAP firmware. It can be recognized by MCUXpresso. But I'm not sure if Ulink pro also has. You can try. If it has, you can see in MCUXpresso

pastedImage_2.png

Regards,

Jing

0 Kudos
Reply

2,947 Views
naasikhendricks
Contributor II

Hi thank you for the reply. ARM promotes coreinsight which is CMSIS DAP and GNU.

µVision Debugger 

I really want to trace but the JTrace is crazy expensive and If i can use it in one environment then i can use it in all the environments.

Kind regards

0 Kudos
Reply