ULinkPro MCUXpress

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ULinkPro MCUXpress

3,135件の閲覧回数
naasikhendricks
Contributor II

Hi I would like to use my UlinkPro to do tracing with Mcuxpress. It is a Eclipse based toolchain and i don't want to mess around too much with current xpress settings.

Kind regards

0 件の賞賛
返信
4 返答(返信)

2,953件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Naasik,

It's not sure. You can try. If the ulinkpro firmware is CMSIS DAP, MCUXpresso can support it. You may ask ARM for help.

Regards,

Jig

0 件の賞賛
返信

2,953件の閲覧回数
naasikhendricks
Contributor II
0 件の賞賛
返信

2,953件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Naasik,

Ulink2 has a CMSIS-DAP firmware. It can be recognized by MCUXpresso. But I'm not sure if Ulink pro also has. You can try. If it has, you can see in MCUXpresso

pastedImage_2.png

Regards,

Jing

0 件の賞賛
返信

2,953件の閲覧回数
naasikhendricks
Contributor II

Hi thank you for the reply. ARM promotes coreinsight which is CMSIS DAP and GNU.

µVision Debugger 

I really want to trace but the JTrace is crazy expensive and If i can use it in one environment then i can use it in all the environments.

Kind regards

0 件の賞賛
返信