Problems with elf File generated by MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with elf File generated by MCUXpresso

Jump to solution
3,765 Views
ChristofAbt
Contributor II

Good afternoon, 

due to problems with the on board debug probe on the FRDM-K66 board and problems of this board with Segger J-Link Plus, I want to use Segger's Ozone and generate the elf file with MCUXPresso. 

After Debug->Start Debug Session -> Download and Reset Program the program should start executing the function main(). The corresponding map file shows that main() starts at 0x428 in the program memory.

extract from frdmk66f_lwip_tcpecho_bm.map

.text.main 0x00000428 0x240 ./source/lwip_tcpecho_bm.o
0x00000428 main

In Ozone at the disassembly window everything looks alright but the code line in the file scope window does not match to the reset conditions. If I understand elf files correctly, the C-code and the corresponding executabble code are linked together. Here, the executable code starts at the right position but is not linked to the corresponding c-code which would be the first non comment or signal declaration line in main().

Thanks in advance for your help

Christof Abt

0 Kudos
Reply
1 Solution
3,723 Views
ChristofAbt
Contributor II

Hello all, 

I have just found out a working designflow with the FRDM-K66F evaluation board. The on board debugger often dies when the board is connected to a Windows 10 computer. I think it is a problem with the software on the additional microcontroller on the board. 

I connected a SEEGER J-link and the connection was established but afterwards the whole system stalled. Yesterday I updated the MCUXpresso IDE to version 24.12.148 and this combination of an external debugger, the FRDM-K66F and the MCUXpresso seems to work. 

My problem is solved!

Thanks for your support

View solution in original post

4 Replies
3,761 Views
ChristofAbt
Contributor II

Sorry, I have forgotten to add the screenshot

ResetOzone.PNG

0 Kudos
Reply
3,724 Views
ChristofAbt
Contributor II

Hello all, 

I have just found out a working designflow with the FRDM-K66F evaluation board. The on board debugger often dies when the board is connected to a Windows 10 computer. I think it is a problem with the software on the additional microcontroller on the board. 

I connected a SEEGER J-link and the connection was established but afterwards the whole system stalled. Yesterday I updated the MCUXpresso IDE to version 24.12.148 and this combination of an external debugger, the FRDM-K66F and the MCUXpresso seems to work. 

My problem is solved!

Thanks for your support

3,719 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello,

I am glad to hear that.  Any new issues, welcome to create a new post.

BRs,

Celeste

0 Kudos
Reply
3,731 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @ChristofAbt ,

Thanks for your post. We don't have Ozone on our side, so I'm unable to replicate your issue in the exactly same way. I used the on-board debugger to debug the axf file generated by MCUXPresso and didn't encounter any problems.

In the .map file:

.text.main 0x000005fc 0x188 ./source/lwip_tcpecho_bm.o

0x000005fc main

Celeste_Liu_0-1743585925978.png

Through the disassembly in the following way.

Celeste_Liu_2-1743586080853.png

 

You can see from the following picture that there is no problem.  

Celeste_Liu_3-1743586356769.png

 

You mentioned that your ELF file was generated by MCUXpresso. Could you please tell me how exactly you generated it?

BRs,

Celeste

0 Kudos
Reply