MCU-LINK-MR firmware update following instructions failed, bricked debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCU-LINK-MR firmware update following instructions failed, bricked debugger

337 次查看
eldar_777
Contributor I

Was trying to update MCU-LINK-MR firmware update following instructions:

https://docs.nxp.com/bundle/UM12219/page/topics/installation_and_firmware_options.html

It failed, now I can not use debugger, even if I press ISP mode button, i can not load firmware, linkserver does not recognize debugger.

0 项奖励
回复
1 回复

319 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @eldar_777 

Please follow the steps below.

Please press the “LPC ISP mode” button and connect the USB to the PC simultaneously. After powering the MCU-Link MR, release the button. The red STATUS LED (LED1) should light and stay on. The board enumerates on the host computer.

Navigate to the MCU-LINK_installer\scripts sub-directory, then run the program_CMSIS.cmd script, following the installation instructions from this script. After updating the firmware, unplug the board from the host computer, then reconnect the board.

 

BR

Alice

0 项奖励
回复