MCUXPRESSO GUI Flash tool issue in Windows10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXPRESSO GUI Flash tool issue in Windows10

1,225 次查看
jeremygeslin
NXP Employee
NXP Employee

Hi,

We recently noticed issues using GUI Flash Tool inside MCUXpresso while running in Windows10 (also reported by several customer).

The operation fails with error "Nn(05). Wire ACK Wait in DAP access".

Below is the complete error log:

pastedImage_7.png

However it is possible, in the same conditions, to flash using the Debug function.

On some laptops the issue is 100% reproducible while on some others it is only observed when the CMSIS-DAP probe (on-board or LPC-Link2) is connected behind an USB hub.

Regards,

Jeremy.

标签 (1)
0 项奖励
回复
1 回复

1,128 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Jeremy - we will contact you directly to obtain more information.

Regards,

MCUXpresso IDE Support

0 项奖励
回复