MCUXPRESSO GUI Flash tool issue in Windows10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXPRESSO GUI Flash tool issue in Windows10

1,255件の閲覧回数
jeremygeslin
NXP Employee
NXP Employee

Hi,

We recently noticed issues using GUI Flash Tool inside MCUXpresso while running in Windows10 (also reported by several customer).

The operation fails with error "Nn(05). Wire ACK Wait in DAP access".

Below is the complete error log:

pastedImage_7.png

However it is possible, in the same conditions, to flash using the Debug function.

On some laptops the issue is 100% reproducible while on some others it is only observed when the CMSIS-DAP probe (on-board or LPC-Link2) is connected behind an USB hub.

Regards,

Jeremy.

ラベル(1)
0 件の賞賛
返信
1 返信

1,158件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Jeremy - we will contact you directly to obtain more information.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信