LinkServer/LinkFLash problems with Dump command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LinkServer/LinkFLash problems with Dump command

Jump to solution
3,097 Views
mimlo
Contributor IV

Hello,
I have a problem with a Save command from LinkServer:

Below you will find a screen from LinkFlash GUI tool from where I can execute Save command (which performs memory dump into a specified .bin file) which works correctly:

mimlo_1-1749549531814.pngmimlo_1-1749549531814.png

However, if I perform the same command from terminal as in the Commands section on the bottom of the picture above, I get a following error (bottom part of the picture below):

mimlo_2-1749549775030.pngmimlo_2-1749549775030.png

I copy pasted the command from LinkFlash to the terminal, I also checked for some invisible characters that could be copied along the way. There were none, string was proper.

Any ideas?

Best regards,
Michael

0 Kudos
Reply
1 Solution
3,068 Views
mayliu1
NXP Employee
NXP Employee

Hi @mimlo ,

Thank you so much for your interest in our products and for using our community.

I did a test for your question,  I'm having the same problem as you.

Then I modify the save command as following, it works, Please try it.

mayliu1_0-1749634262924.pngmayliu1_0-1749634262924.png

I will also escalate your question internally.

Thanks for  raising  this issue.

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

View solution in original post

0 Kudos
Reply
3 Replies
3,045 Views
mimlo
Contributor IV

Hi @mayliu1,
Thanks for this, did not think about trying to revert the arguments.
That worked for me as well, thanks!

0 Kudos
Reply
3,028 Views
mayliu1
NXP Employee
NXP Employee

You are welcome.

 

0 Kudos
Reply
3,069 Views
mayliu1
NXP Employee
NXP Employee

Hi @mimlo ,

Thank you so much for your interest in our products and for using our community.

I did a test for your question,  I'm having the same problem as you.

Then I modify the save command as following, it works, Please try it.

mayliu1_0-1749634262924.pngmayliu1_0-1749634262924.png

I will also escalate your question internally.

Thanks for  raising  this issue.

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 Kudos
Reply