LPCXpressoActivationcode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpressoActivationcode

Jump to solution
3,025 Views
Gene_A
Contributor I


お世話になります。
Gene_Aと申します。

(Below you'll find the English translation.)

表題の件で、質問があります。
LPCXpresso のActivationCodeの取得のためのHPへ接続することが出来ません。
LPCXpresso上からリンクを辿ると下記のアドレスになるのですが、
ページが見つかりませんというエラーとなります。
<https://www.nxp.jp/lpcxpresso/activate>
上記のリンク以外でActivationCodeを発行する方法はあるのでしょうか。

現状、少し前に開発されたソースコードを使用して新規の案件をスタートさせようとしています。
その際に、客先との契約の関係で、開発環境を変えることが出来ず、古い環境を再現する必要があります。
LPCXpresso V7.0.0.を使用する必要があり、その際に上記のActivationCodeが必要になります。
どうかお知恵をお貸し頂ければ幸いです。

(english)
I have a question regarding the subject.
I cannot connect to the website to obtain the LPCXpresso Activation Code.
When I follow the link from LPCXpresso, I get the address below, but I get an error saying the page cannot be found.
<https://www.nxp.jp/lpcxpresso/activate>
Is there a way to issue an Activation Code other than the above link?

Currently, I am trying to start a new project using source code developed a while ago.
Due to a contract with the client, I cannot change the development environment and need to reproduce the old environment.
I need to use LPCXpresso V7.0.0., which requires the above Activation Code.


I would appreciate your advice.

0 Kudos
Reply
1 Solution
3,019 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gene_A,

I tested the registration process, there is no issue. 
So could you try it again with following instruction:

If you can't log in automatically with the IDE generated activation code, navigate to https://lpcxpresso-activation.nxp.com, and enter the product’s serial number. 
 
Hope this helps,
Jun Zhang
 

View solution in original post

0 Kudos
Reply
2 Replies
3,020 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gene_A,

I tested the registration process, there is no issue. 
So could you try it again with following instruction:

If you can't log in automatically with the IDE generated activation code, navigate to https://lpcxpresso-activation.nxp.com, and enter the product’s serial number. 
 
Hope this helps,
Jun Zhang
 
0 Kudos
Reply
2,972 Views
Gene_A
Contributor I

Hi Jun Zhang,

Thank you for your response.
I activated it using the link you provided,
and it completed successfully.
It seems the link I was trying to open with LPCXpresso was old.
(Probably because I was using an old version)

Thank you very much.

Gene_A

0 Kudos
Reply