Is there a tool to help generate Device Configuration Data for the iMXRT series?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a tool to help generate Device Configuration Data for the iMXRT series?

ソリューションへジャンプ
2,102件の閲覧回数
jaldridge
Contributor II

The DCD block is used with execute in place flash and the hard-coded boot loader.

I've been exploring changing the ahb system clock from it's default of 500 MHz to 396 MHz for the industrial temperature version of the MIMXRT1021. I may also need to change the configuration at boot time. Is there an output option from the CLKS tool to generate DCD data? (I've looked but couldn't find it).

タグ(1)
0 件の賞賛
返信
1 解決策
1,973件の閲覧回数
CJarvis
NXP Employee
NXP Employee

DCD support is coming in the next release of the MCUXpresso Config Tools.  It should be available sometime in early June 2019.

元の投稿で解決策を見る

1 返信
1,974件の閲覧回数
CJarvis
NXP Employee
NXP Employee

DCD support is coming in the next release of the MCUXpresso Config Tools.  It should be available sometime in early June 2019.