How yo change CPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How yo change CPU

跳至解决方案
1,579 次查看
_Ferrari_
Contributor V

Dear all,

I developed a project based on LPC5525JDB100 CPU.

The project is almost completed but I have to change the CPU and I have to move to LPC5528JDB100.

The project was develped with MCUXpresso IDE v11.7.1_9221. How to change the CPU in the IDE ?

Thank you very much for your help and cooperation

regards

 

0 项奖励
回复
1 解答
1,508 次查看
danielholala
Senior Contributor II

Hi, @_Ferrari_ 

yo my man, mind correcting the title of your first posting, please? This should be possible through editing the post.

Back to the subject, what @ZhangJennie  did not tell you that this process is not straight forward and is not yet fully automated.

You should read this description, most of all so you do not fall into the trap to keep ”Preserve memory configuration” checked. It is checked by default for no reason.

Hope that helps.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,509 次查看
danielholala
Senior Contributor II

Hi, @_Ferrari_ 

yo my man, mind correcting the title of your first posting, please? This should be possible through editing the post.

Back to the subject, what @ZhangJennie  did not tell you that this process is not straight forward and is not yet fully automated.

You should read this description, most of all so you do not fall into the trap to keep ”Preserve memory configuration” checked. It is checked by default for no reason.

Hope that helps.

0 项奖励
回复
1,538 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi _Ferrari_ 

To change MCU, right click on "MCU" under the project, "Edit MCU".

ZhangJennie_0-1696763978213.png

Have a nice day,

Jun Zhang

0 项奖励
回复