Problems window warning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems window warning

6,719 Views
vijo
Contributor III

Hi there,

pls see attached screen dump

Signal I2C serial clock of the peripheral FLEXCOMM4 is not routed ...........

Under pheripheral signals I have selected PIO0_19 for serial CLOCK, and PIO0_18 for serial DATA.

CONFIG TOOL version 6.

What is causing the warning ?

regards

Viggo

Labels (1)
0 Kudos
Reply
3 Replies

6,582 Views
marek-trmac
NXP Employee
NXP Employee

Hi Viggo,

this validations are done in Peripherals tool. If you have configured FLEXCOMM4 to certain mode, it recommends to route corresponding pins needed in the mode, to ensure peripheral works well.

If this answer does not help, please provide a configuration file (*.mex), so we can analyze details.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

6,582 Views
vijo
Contributor III

Hi Marek,

the warnings only shows up in Config Tool v6. Not in v4.1 see inserted pictures.

How to attach files in a reply ?

Regards

Viggo

Config tool v6 warnings.JPG

Config tool v4.1 no warnings.JPG

0 Kudos
Reply

6,582 Views
marek-trmac
NXP Employee
NXP Employee

> How to attach files in a reply ?
Reply - Use advanced editor (see link top right) - Attach (see link bottom left)

Regards, Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply