MCUXpresso Software Development Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Software Development Kit

3,036件の閲覧回数
saeidsaeidi
Contributor I

Hi,

I am trying to download "MCUXpresso Software Development Kit", however after many times trying, it seems that there is a Problem with the download link?

Thanks and regards!

Saeid

4 返答(返信)

2,663件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Saeid,

this community is related to MCUXpresso Config Tools.

Here is the link to SDK community: https://community.nxp.com/community/mcuxpresso/kinetis-software-development-kit

To download SDK v2.x use http://mcuxpresso.nxp.com/

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信

2,663件の閲覧回数
saeidsaeidi
Contributor I

Hi Carlos,

thank you very much for the Information. In fact I would like to download the MCUXpresso Software Development Kit (SDK) which is described here:

http://www.nxp.com/products/developer-resources/run-time-software/mcuxpresso-software-and-tools/mcux...

I used the download link:

http://www.nxp.com/products/developer-resources/run-time-software/mcuxpresso-software-and-tools/mcux...

However there is no download file available.

It should be an aternative to IAR tool?

The link for the SDK Builder works fine and I could generate a configuration for the microcontroller and use it in IAR. But I am looking for free aternative SDK to IAR.

Best regards

Saeid

0 件の賞賛
返信

2,663件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Saeid,

 

There should not be a download link since the SDK package needs to be built specifically for your processor, evaluation board, OS, IDE and with the needed middleware in order to download it. This seems to be a problem with the webpage, I will report is to our web team.
If you want to use the SDK with IAR then you should select IAR as IDE in the configuration settings:
pastedImage_1.png
Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,663件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Saeid,

Which error do you get while trying to download it?

Are downloading the SDK package from this page?

Welcome to MCUXpresso | MCUXpresso Config Tools 

Please take a look at this guide on how to generate a SDK package:

https://community.nxp.com/docs/DOC-333304 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer