LPC54102 CTIMER Capture Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54102 CTIMER Capture Configuration

2,784件の閲覧回数
BTaylor
Contributor III

How can one use ConfigTools to configure input capture for a CTIMER? I cannot find anywhere in the tool where I can setup a capture input (channel, edge, etc.). Is this a case where I simply need to eschew the tool and configure things manually?

0 件の賞賛
返信
4 返答(返信)

2,761件の閲覧回数
BTaylor
Contributor III

I understand now that ConfigTools does not support Counter mode. It also seems, though, that it does not fully support Capture/Match mode either. It allows match channels to be configured, but I do not see any way to configure capture channels.

0 件の賞賛
返信

2,756件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi BTaylor 

Match channel and capture channel are configured here: There are yellow  exclamation marks on the screenshot because the related pin is not routed. User needs to go to pin configuration tool to config the pin.

ZhangJennie_2-1672114042740.pngZhangJennie_2-1672114042740.png

 

Have a nice day,

Jun Zhang

 

 

0 件の賞賛
返信

2,752件の閲覧回数
BTaylor
Contributor III
With which version of MXUXpresso (and ConfigTools) are you testing? The version I have does not have the 'Capture' section.
0 件の賞賛
返信

2,766件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi BTaylor 

Please refer answer in this thread

https://community.nxp.com/t5/MCUXpresso-Config-Tools/LPC54102-CTIMERx-in-Counter-Mode/td-p/1573949

Thanks,

Jun Zhang

0 件の賞賛
返信