blhost does not work on Ubuntu 16.04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

blhost does not work on Ubuntu 16.04

2,289 次查看
dugg
Contributor II

I'm using blhost on Ubuntu16.04 and I have made sure that all dependencies required in the manual such as libudev.so.1, libc.so.6, etc are all installed and can be found on system path. But when I run

    sudo blhost -p COM1 -- get-property 1

It reports an error

"Could not open serial port.Error: UartPeripheral() cannot open PC UART port(COM1), speed(57600 Hz)."

What's the problem here?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

1,915 次查看
wilkinsw
Contributor III

COM ports are for Windows, try replacing "COM1" with /dev/ttyUSB0 or /dev/ttyAMC0 depending on the output of

ls /dev/tty*

0 项奖励
回复

1,915 次查看
dugg
Contributor II

Hi Mike,

I used the board we developed ourselves with the K64F12.

and i'm sure there is no problem with the board.because i was successful on win7 systems .

0 项奖励
回复

1,915 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Sorry for the later reply.

Which board you are using with KBOOT blhost tool?

Thanks with regards,

Mike

0 项奖励
回复

1,915 次查看
dugg
Contributor II

Hi Mike,

I used the board we developed ourselves with the K64F12.

and i'm sure there is no problem with the board.because i was successful on win7 systems .

0 项奖励
回复