RT1021 -- blhost to query flash ID to enable the coresponding QE bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1021 -- blhost to query flash ID to enable the coresponding QE bit

ソリューションへジャンプ
2,669件の閲覧回数
JamesNgo
Contributor III

My RT1021 based design supports several compatible spiFlash types and vendors. Each of these flash parts has the QE bit at different position, apparently shown below:

JamesNgo_0-1695412386008.png

 

Questions:

1. BLHOST does not seem to have a command or method to query the flash parts ID/vendor to configure Quad Enable bit appropriately. It appears it is OK under the assumption that the system design supports 1 flash type at a time. If different part is used in the system, BLHOST scripts have to be changed to work with a different part. Please confirm this.

2. Given (1) is true, is there any option to query the flash part ID (during runtime) to enable the QE bit appropriately for design that supports multiple compatible flash parts?

 

Thanks

-james

 

0 件の賞賛
返信
1 解決策
2,493件の閲覧回数
JamesNgo
Contributor III

Hi Pavel,

I couldn't generate the IVT_flashloader.bin as I described earlier due to the unknown reason it couldn't read the input file.bin. So I explored other options...

And I found one working option that I'd like to share the findings to benefit all other fellows here who may be interested.

Technically the IVT has the boot info that the SPDHOST needs to "jump". I managed to INCLUDE the entire IVT into the flashloader.bin on the top image in the code (as if elftosb would have worked) -- hence I do NOT have to use the "elftosb" to generate it.

Preprocessor:

XIP_BOOT_HEADER_DCD_ENABLE=1
XIP_BOOT_HEADER_ENABLE = 1

linker.icf

define symbol __ram_vector_table_size__ = isdefinedsymbol(__ram_vector_table__) ? 0x00000400 : 0;
define symbol __ram_vector_table_offset__ = isdefinedsymbol(__ram_vector_table__) ? 0x000003FF : 0;

define symbol m_interrupts_ram_start = 0x20000000;
define symbol m_interrupts_ram_end = 0x20000000 + __ram_vector_table_offset__;

define symbol m_data_start = m_interrupts_ram_start + __ram_vector_table_size__;
define symbol m_data_end = 0x2000FFFF;

define symbol m_data2_start = 0x20200000;
define symbol m_data2_end = 0x20207FFF;

define symbol m_interrupts_start = 0x2020A000;
define symbol m_interrupts_end = 0x2020A3FF;
define symbol m_text_start = 0x2020A400;
define symbol m_text_end = 0x2021FFFF;


define exported symbol m_boot_hdr_conf_start = 0x20208000;
define symbol m_boot_hdr_ivt_start = 0x20209000;
define symbol m_boot_hdr_boot_data_start = 0x20209020;
define symbol m_boot_hdr_dcd_data_start = 0x20209030;

//place at address mem: m_interrupts_start { readonly section .intvec };
place at address mem: m_boot_hdr_conf_start { section .boot_hdr.conf };
place at address mem: m_boot_hdr_ivt_start { section .boot_hdr.ivt };
place at address mem: m_boot_hdr_boot_data_start { readonly section .boot_hdr.boot_data };
place at address mem: m_boot_hdr_dcd_data_start { readonly section .boot_hdr.dcd_data };

keep{ section .boot_hdr.conf, section .boot_hdr.ivt, section .boot_hdr.boot_data, section .boot_hdr.dcd_data };

 

SPDHOST scripts:

sdphost.exe -u 0x1fc9,0x0130 -- write-file 0x20208000 ivt_builtin_flashloader.bin
sdphost.exe -u 0x1fc9,0x0130 -- jump-address 0x20209000

Thanks.

-James

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,532件の閲覧回数
JamesNgo
Contributor III

Hi Pavel,

To continue pursuing the solution I mentioned above, I need to generate the ivt_flashloader.bin (?!) that is for the SDPHOST to write to 0x202A000 (and jump to 0x2020A400) to execute. And after this, flashloader will execute. Please help review my simple steps below to see if there's anything missing/wrong:

Now, IAR generates the flashloader.srec as shown below:

JamesNgo_0-1695935407748.png

I'm using imx-dtcm-unsigned.bd

JamesNgo_1-1695935504751.png

 

Use ELFTOSB to generate the final BIN with the following command:

elftosb.exe -f imx -V -c imx-dtcm-unsigned.bd -o ivt_flashloader.bin flashloader.srec‍‍‍‍‍‍‍‍‍

Here's the problem:

JamesNgo_2-1695935649814.png

thanks

0 件の賞賛
返信
2,494件の閲覧回数
JamesNgo
Contributor III

Hi Pavel,

I couldn't generate the IVT_flashloader.bin as I described earlier due to the unknown reason it couldn't read the input file.bin. So I explored other options...

And I found one working option that I'd like to share the findings to benefit all other fellows here who may be interested.

Technically the IVT has the boot info that the SPDHOST needs to "jump". I managed to INCLUDE the entire IVT into the flashloader.bin on the top image in the code (as if elftosb would have worked) -- hence I do NOT have to use the "elftosb" to generate it.

Preprocessor:

XIP_BOOT_HEADER_DCD_ENABLE=1
XIP_BOOT_HEADER_ENABLE = 1

linker.icf

define symbol __ram_vector_table_size__ = isdefinedsymbol(__ram_vector_table__) ? 0x00000400 : 0;
define symbol __ram_vector_table_offset__ = isdefinedsymbol(__ram_vector_table__) ? 0x000003FF : 0;

define symbol m_interrupts_ram_start = 0x20000000;
define symbol m_interrupts_ram_end = 0x20000000 + __ram_vector_table_offset__;

define symbol m_data_start = m_interrupts_ram_start + __ram_vector_table_size__;
define symbol m_data_end = 0x2000FFFF;

define symbol m_data2_start = 0x20200000;
define symbol m_data2_end = 0x20207FFF;

define symbol m_interrupts_start = 0x2020A000;
define symbol m_interrupts_end = 0x2020A3FF;
define symbol m_text_start = 0x2020A400;
define symbol m_text_end = 0x2021FFFF;


define exported symbol m_boot_hdr_conf_start = 0x20208000;
define symbol m_boot_hdr_ivt_start = 0x20209000;
define symbol m_boot_hdr_boot_data_start = 0x20209020;
define symbol m_boot_hdr_dcd_data_start = 0x20209030;

//place at address mem: m_interrupts_start { readonly section .intvec };
place at address mem: m_boot_hdr_conf_start { section .boot_hdr.conf };
place at address mem: m_boot_hdr_ivt_start { section .boot_hdr.ivt };
place at address mem: m_boot_hdr_boot_data_start { readonly section .boot_hdr.boot_data };
place at address mem: m_boot_hdr_dcd_data_start { readonly section .boot_hdr.dcd_data };

keep{ section .boot_hdr.conf, section .boot_hdr.ivt, section .boot_hdr.boot_data, section .boot_hdr.dcd_data };

 

SPDHOST scripts:

sdphost.exe -u 0x1fc9,0x0130 -- write-file 0x20208000 ivt_builtin_flashloader.bin
sdphost.exe -u 0x1fc9,0x0130 -- jump-address 0x20209000

Thanks.

-James

0 件の賞賛
返信
2,545件の閲覧回数
JamesNgo
Contributor III

Hi Pavel,

I have some updates from my end... I tried EVK-MIMXRT1020-flexspi_nor_polling_transfer on internal RAM with some additional flexspi accessing LUTs and can query various flash parts ID. From this info, the respective QE bit of the flash part can be enabled.

I assume I can pull in or merge this code base into RAM "flashloader" to add to the BLHOST "configure-memory" option (at least the supported flash types auto-detection in order to set the corresponding QE bit appropriately). And this is the solution I'm pursuing. 

0 件の賞賛
返信
2,577件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

Best regards,
Pavel

0 件の賞賛
返信