LPC4074 access on chip flash write/read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4074 access on chip flash write/read

1,854 Views
Jackson7781
Contributor I

 

Spoiler
Hi everyone. 
I'm new, I'm recently working on a Lpc4074 project, I want to  access flash for bootloader  application, is there any related resource that I can implement this  ?

thank you very much



 

0 Kudos
Reply
1 Reply

1,840 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jackson7781 

The on board boot rom code is never open to external.

If you want to develop your own secondary bootloader, we don't have exact demo for LPC4074, but you can refer  it as well.

SPI secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11257.zip

I2C secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11258.zip

LPC1700 secondary USB bootloader
https://www.nxp.com/docs/en/application-note/AN10866.zip

These ANs are based on LPC17xx but motherd is the same for LPC40xx


This AN is Migrating from the LPC177x/8x to LPC407x/8x, in case you need it.
https://www.nxp.com/docs/en/application-note/AN11335.zip

 

Thanks,

Jun Zhang

0 Kudos
Reply