LPC4074 access on chip flash write/read

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4074 access on chip flash write/read

2,358 次查看
Jackson7781
Contributor I

 

破坏者
Hi everyone. 
I'm new, I'm recently working on a Lpc4074 project, I want to  access flash for bootloader  application, is there any related resource that I can implement this  ?

thank you very much



 

0 项奖励
回复
1 回复

2,344 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jackson7781 

The on board boot rom code is never open to external.

If you want to develop your own secondary bootloader, we don't have exact demo for LPC4074, but you can refer  it as well.

SPI secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11257.zip

I2C secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11258.zip

LPC1700 secondary USB bootloader
https://www.nxp.com/docs/en/application-note/AN10866.zip

These ANs are based on LPC17xx but motherd is the same for LPC40xx


This AN is Migrating from the LPC177x/8x to LPC407x/8x, in case you need it.
https://www.nxp.com/docs/en/application-note/AN11335.zip

 

Thanks,

Jun Zhang

0 项奖励
回复