Kinetis Bootloader 2.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Bootloader 2.0.0

1,774 Views
sunnywu
Contributor II

Why the Kinetis Bootloader 2.0.0 can't support the KE06 serials,  the better, it can support all the Kinets serials for the customer, the good bootloader is very important.

0 Kudos
Reply
1 Reply

1,633 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Wu,

Yes, none of KE0x and KEA series devices has ROM bootloader, flashloader, and flash-resident bootloader. If customer want to use flash bootloader, they have to port it by themselves. I'm not sure why. I guess this is because many of KE/KEA usage is auto and high reliable control. Bootloader 2.0.0 isn't fit for such case. But yes, in many other application, bootloader is useful. But it seems there isn't such a plan.

Regards,

Jing

0 Kudos
Reply