In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

3,281 Views
NVazquez
Contributor IV

In device manager, USB on custom board for LPC54016 shows "LPC" in "Universal Serial Bus Device" instead of showing as "HID-Compliant vendor-defined device".

 

The Driver it is using is WinUsb Device. I don't think that is right and it should use hidusb.sys driver. The USB connector is connected to USB0 of the LPC54016. 

0 Kudos
Reply
4 Replies

3,258 Views
NVazquez
Contributor IV

I tried with an HID example from SDK and I am able to see my board under "Human Interface Device" as "HID-Compliant device".

0 Kudos
Reply

1,993 Views
daihhqn
Contributor I

Could you please share me the HID? 

Thanks!

0 Kudos
Reply

3,265 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I agree with that the PC should use the hidusb.sys driver for HID class.

BR

XiangJun Rong

0 Kudos
Reply

1,994 Views
daihhqn
Contributor I

Could you please share me official hidusb.sys to connect iMX6 devices

0 Kudos
Reply