In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

3,378 次查看
NVazquez
Contributor IV

In device manager, USB on custom board for LPC54016 shows "LPC" in "Universal Serial Bus Device" instead of showing as "HID-Compliant vendor-defined device".

 

The Driver it is using is WinUsb Device. I don't think that is right and it should use hidusb.sys driver. The USB connector is connected to USB0 of the LPC54016. 

0 项奖励
回复
4 回复数

3,355 次查看
NVazquez
Contributor IV

I tried with an HID example from SDK and I am able to see my board under "Human Interface Device" as "HID-Compliant device".

0 项奖励
回复

2,090 次查看
daihhqn
Contributor I

Could you please share me the HID? 

Thanks!

0 项奖励
回复

3,362 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I agree with that the PC should use the hidusb.sys driver for HID class.

BR

XiangJun Rong

0 项奖励
回复

2,091 次查看
daihhqn
Contributor I

Could you please share me official hidusb.sys to connect iMX6 devices

0 项奖励
回复