How long does blhost take to flash image normally?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How long does blhost take to flash image normally?

1,822 次查看
tonymakkiel
Contributor III

Hi,

    I am trying to flash KL17 board using blhost (bootloader 2.0.0). It takes almost an hour (53 minutes) to flash a hex file of size 215243Bytes (ie 68B/s). Is it normal? Or am I missing something?

The command used is

./blhost  -p /dev/ttyUSB0,115200 flash-image img_twrkl43z48m.hex erase

 

Many Thanks,

Tony

标签 (1)
0 项奖励
回复
2 回复数

1,633 次查看
eatonzhang
NXP Employee
NXP Employee

Hi Tony,

It is not normal. The real speed should be lower than the theoretical one, but it shouldn't be such low.

But I tried to flash 32KB data into KL17, it costs 9.7s on Windows, 14.5s on Linux.

My Linux system is Ubuntu 14.10 32bits under Virtual Box.

I'm not sure if it is your OS's issue. Could you please re-try on other PCs?

Best Regards,

Yitao

0 项奖励
回复

1,633 次查看
tonymakkiel
Contributor III

Thank you Yitao. I will try on different OS(and PC) and update the result.

0 项奖励
回复