How long does blhost take to flash image normally?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How long does blhost take to flash image normally?

2,468件の閲覧回数
tonymakkiel
Contributor III

Hi,

    I am trying to flash KL17 board using blhost (bootloader 2.0.0). It takes almost an hour (53 minutes) to flash a hex file of size 215243Bytes (ie 68B/s). Is it normal? Or am I missing something?

The command used is

./blhost  -p /dev/ttyUSB0,115200 flash-image img_twrkl43z48m.hex erase

 

Many Thanks,

Tony

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,279件の閲覧回数
eatonzhang
NXP Employee
NXP Employee

Hi Tony,

It is not normal. The real speed should be lower than the theoretical one, but it shouldn't be such low.

But I tried to flash 32KB data into KL17, it costs 9.7s on Windows, 14.5s on Linux.

My Linux system is Ubuntu 14.10 32bits under Virtual Box.

I'm not sure if it is your OS's issue. Could you please re-try on other PCs?

Best Regards,

Yitao

0 件の賞賛
返信

2,279件の閲覧回数
tonymakkiel
Contributor III

Thank you Yitao. I will try on different OS(and PC) and update the result.

0 件の賞賛
返信