Help! Need the correct openocd configuration for KEAZ128.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help! Need the correct openocd configuration for KEAZ128.

跳至解决方案
1,721 次查看
millerlowe
Contributor II

Hi Folks,

We're using a KEAZ128 processor on a new project and I am currently trying to bring tool up with gdb on openocd using a CMSIS_DAP SWD adapter.  We use these tools for several other K and LPC series targets.

The info page says:

  • GDB debugger with support for the following debug interface hardware:
    • SEGGER J-Link (w/SEGGER GDB Server, Windows, Linux, Mac)
    • P&E Multilink (w/P&E GDB Server, Windows, Linux)
    • CMSIS-DAP (w/OpenOCD GDB and OpenSDA embedded circuit,Windows, Linux)
    • Command Line (CL) debugging with GDB and OpenOCD TCL

But I can't get a working configuration.  Does anyone know the target config to use or have a working custom one?

0 项奖励
回复
1 解答
1,523 次查看
millerlowe
Contributor II

Hi Kerry, 

Your reply in the other post was incorrect as I was able to get my openocd/gdb environment working fine.. I just had to use a later instance of openocd and the ke0x.cfg configuration.  You can see the other thread (as linked in Kerry's post above) for my solutions.

Sorry for posting in two places.

Miller

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,524 次查看
millerlowe
Contributor II

Hi Kerry, 

Your reply in the other post was incorrect as I was able to get my openocd/gdb environment working fine.. I just had to use a later instance of openocd and the ke0x.cfg configuration.  You can see the other thread (as linked in Kerry's post above) for my solutions.

Sorry for posting in two places.

Miller

0 项奖励
回复
1,523 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Miller,

   This question is the same topic as your another post:

Help! Need the correct openocd configuration for KEAZ128. 

  I have replied you in the above post.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复