Help! Need the correct openocd configuration for KEAZ128.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help! Need the correct openocd configuration for KEAZ128.

ソリューションへジャンプ
1,702件の閲覧回数
millerlowe
Contributor II

Hi Folks,

We're using a KEAZ128 processor on a new project and I am currently trying to bring tool up with gdb on openocd using a CMSIS_DAP SWD adapter.  We use these tools for several other K and LPC series targets.

The info page says:

  • GDB debugger with support for the following debug interface hardware:
    • SEGGER J-Link (w/SEGGER GDB Server, Windows, Linux, Mac)
    • P&E Multilink (w/P&E GDB Server, Windows, Linux)
    • CMSIS-DAP (w/OpenOCD GDB and OpenSDA embedded circuit,Windows, Linux)
    • Command Line (CL) debugging with GDB and OpenOCD TCL

But I can't get a working configuration.  Does anyone know the target config to use or have a working custom one?

0 件の賞賛
返信
1 解決策
1,504件の閲覧回数
millerlowe
Contributor II

Hi Kerry, 

Your reply in the other post was incorrect as I was able to get my openocd/gdb environment working fine.. I just had to use a later instance of openocd and the ke0x.cfg configuration.  You can see the other thread (as linked in Kerry's post above) for my solutions.

Sorry for posting in two places.

Miller

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,505件の閲覧回数
millerlowe
Contributor II

Hi Kerry, 

Your reply in the other post was incorrect as I was able to get my openocd/gdb environment working fine.. I just had to use a later instance of openocd and the ke0x.cfg configuration.  You can see the other thread (as linked in Kerry's post above) for my solutions.

Sorry for posting in two places.

Miller

0 件の賞賛
返信
1,504件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Miller,

   This question is the same topic as your another post:

Help! Need the correct openocd configuration for KEAZ128. 

  I have replied you in the above post.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信