How to add a new camera driver for toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a new camera driver for toolbox

6,376 Views
jim_duan
Contributor II

I am trying to using a different camera other than the default one. Can you provide the instructions so that I can add its ISP driver in?

For example, GMSL Camera with OV10635 & Maxim Deserilaizer .. 

Thanks.

Jd

3 Replies

3,895 Views
Nanettebreaux
Contributor I

The MF driver is a driver that is installed for printing, sending faxes, and scanning using a device. As well as the MF driver and MF Scan Utility explained here, other software may be installed depending on the supported device. For details about the other software, refer to the manual of the device. Printer Driver.  

0 Kudos
Reply

6,283 Views
jimduanva
Contributor II

I have made the toolkit working with camera MXOV10635-S32V by replace the original Sony ISP.

6,283 Views
Daniel_Popa
NXP Employee
NXP Employee

nxf40536‌,

Do we have any solutions for this issue?

0 Kudos
Reply