How to get data source directly from CSI?Not through the CSI-SRAM-FDMA-DDR approach

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get data source directly from CSI?Not through the CSI-SRAM-FDMA-DDR approach

8,555 Views
fgd455464199
Contributor I

Isp_csi_dcu routine development, using different types of cameras, how can more directly get the camera information?

0 Kudos
Reply
4 Replies

6,831 Views
Bessieswsa
Contributor I

Thankful for the little by little useful exercise. Has conclusively the ordinary impact!

DG Paystub Portal

0 Kudos
Reply

6,816 Views
Bessieswsa
Contributor I

I totally like your gave limits as the post you passed on has some uncommon information which is totally essential for me.

0 Kudos
Reply

8,291 Views
Stephanynl
Contributor I

So the question basically is already in the title: I am not really finding any reasonable microcontroller with MIPI / CSI interface for interfacing a 2MP image sensor (12-bit RAW format).

There are some Cortex M7 from STM (I think) but considering 1920 x 1080 x 12bit = 3Mbyte of data per picture this seems overkill (maybe I am wrong)?

I neither want to use a Raspi nor an FPGA.

What would you recommend?

 

 

My AARP Medicare

0 Kudos
Reply

8,482 Views
paulvlase
NXP Employee
NXP Employee

Hello 国栋 范 ,

 

This community space do not cover the topic you need assistance on.

Please create new NXP support case according to following procedure:https://community.nxp.com/docs/DOC-329745

 

Hope this helps,

Paul

0 Kudos
Reply