RDK-Demo Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RDK-Demo Controller

8,763 Views
burak_
Contributor II

Hi,

I have installed RDK-demo controller on my windows 10 laptop. But when ı try to run program, nothing happens. Program window does not open. In task manager, the task is running. I tried to run it as administrator, nothing has changed. Who can help me solving this issue?

0 Kudos
Reply
5 Replies

7,581 Views
Iktler
Contributor I

Are there any new solutions? I had exactly the same problem...

0 Kudos
Reply

8,746 Views
longfeiwang
Contributor III

Do you mean it can't be programmed? Or it doesn't run after programming?

0 Kudos
Reply

8,742 Views
burak_
Contributor II

I mean, I cannot open the GUI. When ı double click on icon, the application does not open but it is running on background, ı can see in task manager.

0 Kudos
Reply

8,740 Views
longfeiwang
Contributor III

You need to install the correct version of the matlab runtime environment and set the correct TFTP directory, then you can run app.exe normally.

0 Kudos
Reply

8,711 Views
marmar
Contributor I

I have the same problem. Where should I set the right TFTP directory?

0 Kudos
Reply