License Error : NXP RADAR Toolbox for S32R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License Error : NXP RADAR Toolbox for S32R

ソリューションへジャンプ
8,885件の閲覧回数
Vamsi_Sirigina
Contributor II

Hi, warm Greeting!! , Could you please me on below issue 

I have installed  NXP RADAR SPT toolbox 3.0x 1.7.0 version

matlab version 2022b.

facing license error : 

Vamsi_Sirigina_0-1694648834825.png

#MBDT  

0 件の賞賛
返信
1 解決策
8,774件の閲覧回数
Vamsi_Sirigina
Contributor II

Great!!!!Thank you @iulianbulancea ..:) 

it working fine now 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
8,815件の閲覧回数
Vamsi_Sirigina
Contributor II
>> example_add_mex_spt31
Error using pbrstg
Flexnet failed to check the license:
1) For feature "MBD_Toolbox_SPT_3.0" due to:NOFEATURE - No such feature exists.
Error in example_add_mex_spt31 (line 60)
switch_spt(31);
License.dat
#Model-Based Design for SPT - Model-Based Design Toolbox for S32 SPT 3.x 1.7.0
#for vamsi sirigina Software Account
# License for DISK_SERIAL_NUM=XXXXXXXXXX
INCREMENT MBD_Toolbox_SPT freescale 1.0 25-feb-2033 uncounted \
VENDOR_STRING="Model-Based Design Toolbox for S32 SPT 3.x \
1.7.0" HOSTID=DISK_SERIAL_NUM=8c74f48f ISSUER="Freescale \
Semiconductor" ISSUED=13-sep-2023 ck=186 SN="FSL - 3355348" \
TS_OK SIGN="14B9 B8F0 CAD6 A593 C28F C850 65B6 339C 7D72 841F \
F584 D329 F3FC 4B6D E43E 0F5F 8AFB 69F3 59E2 D62B 97FC 366A \
8B5C 045D 975C 590C 3AF5 3601 DA41 BAA7"
 
Thankyou @iulianbulancea 
0 件の賞賛
返信
8,782件の閲覧回数
iulianbulancea
NXP Employee
NXP Employee

Hello @Vamsi_Sirigina ,

Can you install a patch of the toolbox found here? Please save and use the license file that you have.

Thank you,

Iulian Bulancea

8,775件の閲覧回数
Vamsi_Sirigina
Contributor II

Great!!!!Thank you @iulianbulancea ..:) 

it working fine now 

0 件の賞賛
返信
8,835件の閲覧回数
iulianbulancea
NXP Employee
NXP Employee

Hello @Vamsi_Sirigina ,

Can you run example_add_mex_spt31.m and send me the error?

Also, can open the license file and send me the license feature? The feature is a word in the license file that you can find here:

temp.jpg

Thank you,

Iulian Bulancea

0 件の賞賛
返信