Linux Embedded Challenge Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Embedded Challenge Knowledge Base

Discussions

Sort by:
Our project is Adaptive Cruise Control and for our first milestone we built a proof-of-concept automobile which can be controlled from a computer with the help of an application. In this app the speed can be adjusted and the car can be controlled using the WASD keys. Also, it has the option of cruise control which moves the car forward at a constant speed.
View full article
Milestone_1 Implementarea hardware si software; Aplicatia grafica a sistemului: ofera o vedere top-down a intersectiilor si a celor 2 vehicule; Posibilitatea de a alege punctul de start si punctul de oprire a vehiculelor; Vehiculele incetinesc cand se apropie unul de celalalt pentru a evita coliziunea.
View full article
The robot is assembled and powered from battery. User is able to command the robot wheels from the web interface.
View full article
Am instalat Tomcat 8.5.14 si MySQL server 5.5 pe placuta UdooNeo, apoi am realizat o aplicatie web in Tomcat care sa faca legatura intre o interfata grafica in browser accesabila de catre utilizator si baza de date. Utilizatorul poate cere in request pentru o anumita data, ora si durata iar daca nu mai exista in request in acea perioada de timp utilizatorul primeste in cod pe care il poate folosi pentru a accesa serverul in perioada de timp ceruta.
View full article
La acest milestone trebuia sa conectez senzorii la placuta iar acestia sa detecteze miscarea si sa se activeze o alarma.
View full article
For this milestone, the new implemented functionality consists of: - adding login/logout feature - enabling an admin user to add new users - separating devices by users and commands by devices - adding IR learning functionality for devices which use the Sony protocol - lighting up a LED while the device is in learning mode
View full article
We bought the compatible components for our project and tested each of them. GPS module (u-blox NEO-6M + GPS antenna) USB mobile broadband mode In this milestone we also bought a Microsoft Azure subscription for testing and deployment.
View full article
Buna ziua, Pentru primul milestone am conectat o pereche laser-fotorezistor la plăcuța UDOO și am citit valorile analogice (simuland inaltimea produsului final). Multumim !
View full article
We run out of batteries so we used direct alimentation for the demo.
View full article
Am atasat un lcd si am afisat datele citite pe el, am pus mana pe senzorii de temperatura si peste cel de lumina pentru a se observa ca se schimba valorile.
View full article
In acest video,se poate observa cum prin intermediul placutei se acceseaza camera de la telefon.Pe urma se captureaza imaginea cu barcode-ul si se poate observa cum a scanat cu succes codul EAN din care se poate extrage si ISBN-ul.
View full article
In video sunt descrise gesturile corespunzatoare fiecarei actiuni a mouse-ului: mouse movement, left click, right click, normal scroll, fast scroll. PS: Manusa va fi schimbata cu alta mai noua. Videoul a fost inregistrat cu webcamul.
View full article
We implemented an application in c that helps us control the car. We are sending data between cores using serial transmision. We also started to implement a part of the bonus (change direction to avoid obstacles). The source code will be available on git.
View full article
In acest video demonstram prototipul pentru bordul masinii, sistemul de iluminat si mecanismele pentru miscare.
View full article
We show in the video how we managed to connect the circuit, how we made the pwm for different speeds and a little demo with the movement of the car.
View full article
In acest video descriem suportul fizic construit pentru proiect.
View full article
RS Lang Milestone 2: Build the controlling application Build an application that sets the speed of the car at a certain value. The car should be able to move with constant speed and when a new speed value is received from the app, it should accelerate or brake properly.
View full article
Simple web interface for controlling our robot. It contains buttons for movement and a console for robot output.
View full article
In acest filmulet prezentam indeplinirea sarcinilor corespunzatoare primei etape: conectarea senzorilor la placa UDOO.citirea senzorilor(temperatura, umiditate, altitudine, presiune atmosferica si intensitate luminoasa) si afisarea datelor in terminalul Linux. De asemenea, se poate observa ca folosim si un LED care semnalizeaza nivelul de lumina(se aprinde atunci cand nivelul intensitatii scade sub o anumita valoare). Prima parte a filmuletului prezinta realizarea conexiunilor cu placa . Toti senzorii sunt alimentati de la 3.3V conform specificatiilor pentru functionare optima din foile lor de catalog. Totodata, aceasta tensiune este sub pragul de 3.3V ceea ce protejeaza porturile de intrare ale placutei. Conexiunea fizica UDOO - calculator a fost realizata prin USB iar pentru a avea acces la terminal s-a folosit VNC + Putty In partea doua a doua a filmuletului se observa afisarea in consola a datelor citite de la senzori, iar ultima parte reprezinta un bonus prin care dorim sa semnalizam scaderea intensitatii luminoase sub un anumit prag prin aprinderea unei lumini, in cazul de fata un LED.
View full article