Linux Embedded Challenge Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Embedded Challenge Knowledge Base

Discussions

Sort by:
-an administrator would be able to access and configure the applications remotely or locally based on mail and a password authentication method. -it can be done over a remote connection (webserver or phone) bonus activities: -an administrator can add, edit or remove requests using the LCD. -on index page are displayed number of requests,  available hours to be reserved through "Check Available Hours" feature and logs, which can be found in the admin platform. -these statistics can be available locally (on the LCD) or remotely (web or phone)
View full article
Salutare! In acest video se poate observa cum cartea este identificata in functie de codul ISBN si cum aplicatia cere permisiunea de a adauga o carte noua in shelf in numele unui utilizator de  Goodreads. La adaugarea cartii este prezentata optiunea de a alege intre read, curently-reading si to-read. La alegerea primei optiuni se va aprinde LED-ul verde, iar pentru celelalte doua optiuni cel galben, respectiv rosu.
View full article
In this video you can see the effect of various parameters exceeding the thresholds that we set: alerts being displayed. Note: The alert that we were supposed to configure during the bonus milestone was also implemented during this stage. 
View full article
Hello, For the last milestone and the bonus we made the python script to control the car. We take images from the camera and then processing them to determine distance to the car in front of us. Based on that distance, python script adapt the speed of the car, stopping it if it is necessary or avoiding the obstacle. We are sorry for bad demo at bonus but the batteries were over and we ran out of time.
View full article
Project 1: Conveyor Belt with Optical Sorter milestone 1: Codul pentru controlul motoarelor este pe repo-ul de git in folderul src. In faza experimentala este si scriptul de openCV pentru datele primite de la camera. 
View full article
Bună, Pentru Bonusul 2 , o persoană a cântat o melodie la harpă, în timp ce cealaltă persoană a încercat să ghicească melodia , străduindu-se să facă cât mai puține greșeli. 
View full article
Milestone 3 : Build the video camera setup Add a video camera to the system. The controlling application should be able to identify vehicles in front of the car and the distance to them. One alternative to this is to select an object (for example, a vehicle number plate or some other fixed-shape form) and, knowing its dimensions and the camera’s focal properties, estimate the distance to it. It is recommended, but not mandatory, to use OpenCV for image processing.
View full article
Bună , Am făcut Bonusul 1 în care am setat intensitatea unui LED în funcție de înălțimea notei : pentru o notă mai joasă de pe octavă ( DO ) LED-ul va lumina mai puțin , iar pentru o notă mai înaltă ( SI ) , va lumina mai puternic . Astfel , LED-ul are 10 intensitați posibile .  PS :  Pe langa plusul estetic, LED-ul conectat la PWM poate fi folosit și pentru depanare. Mulțumim !
View full article
Salutare! Aceasta este forma finala a proiectului, programul ruland pe placuta UDOO. In prima parte este scanat codul ISBN, apoi este ceruta permisiunea utilizatorului ca programul sa poata adauga informatii in numele lui accesand linkul pus la dispozitie. Pasul urmator este stabilirea statusului cartii (read, reading, to-read), alegand un numar de la 1 la 3, in functie de alegere aprinzandu-se unul dintre cele 3 LED-uri (cel verde in cazul nostru). PS: am taiat filmuletul in momentele incarcarii paginii deoarece dureaza mult
View full article
We described the web interface and its functionality.
View full article
Acest video prezinta modul de utilizare a camera mouse-ului. Am regandit gesturile pe care trebuie sa le faca utilizatorul afisate in Milestone_1. Astfel, utilizatorul trebuie sa miste punctul verde in fata camerei pentru a misca pointerul, sa aproprie punctul verde de camera pentru click stanga si sa-l departeze pentru click dreapta. Inainte de folosirea propriu zisa a camera mouse-ului, camera trebuie calibrata, pentru acuratete maxima in detectarea punctului verde (mai multe detalii in documentatie).
View full article
In acest video este scanat cu ajutorul camerei de la telefon isbn-ul cartii "After you"  si anume,aceasta After You (Me Before You, #2) by Jojo Moyes — Reviews, Discussion, Bookclubs, Lists.Dupa cum se vede este gasita cartea  pe goodreads si se aprinde ledul verde pentru ca am reusit sa scanam,sa ne conectam la goodreads si sa cautam cartea.
View full article
In this milestone we focused on creating the infrastructure that controls the data flow that we receive from the device. We created a Web API application (ASP .NET ) hosted in Google Cloud Platform that stores and interprets our data (that comes from the device) and also sends a notification to the mobile app informing the user that the car is being stolen (it has moved). We also created the mobile app (native, created in Xamarin.Android) that consumes the Google Maps API in order to embed a map fragment that we use to display the position of our device (and implicitly, the position of the car). The notification system is production ready, in the way that we use Azure Notification Hub as a middleware for passing notifications because it's scalable, reliable, contains telemetry and it's also secure.
View full article
Implemented infrared transmitter with SONY protocol, such that the user can: - directly trigger a SONY device command from the web interface - schedule a SONY device command to trigger at a future time (just once or daily) from the web interface
View full article
Bonus activity (20 pts): Obstacle Avoidance The system could include a new feature for automatic obstacle avoidance. The car will be able to change its direction when breaking is not enough to avoid collision or when it detects static objects. Change directions as if the car is switching lanes (i.e. go in one way and immediately in the other, so as to pass the obstacle parallel to your initial trajectory).
View full article
In acest video se prezinta conectarea la API-ul Goodreads iar faptul ca ledul verde se aprinde inseamna ca conectarea a reusit.
View full article
Hello everyone, In this video we are showing off a couple of new features we implemented for the third Milestone. Yoda can notify you when there is some activity in your house or a gas leak occurs. Yoda can monitor disabled or elder ones, keep in touch with them and remind them to take medication. If the person does not answer, a notification is sent to the user. For more details about implementation, installation instructions and other specifications, please check our Git repository. Thanks for watching, Team Yoda
View full article
Hello everyone, In this video we are showing off the Android application we implemented as a bonus. The virtual assistant program running on the UDOO Quad is also a web server which exposes a very basic REST API. This API is used to remotely control the assistant. The Android application uses Google's STT API to convert speech-to-text, send the input over internet to Yoda, who processes the input and sends back an answer, which is rendered using Google's TTS API. All plugins demonstrated in previous videos are usable from the Android application since the mobile phone is just another I/O and all the processing is still done by the application running on UDOO board. For more details about implementation, installation instructions and other specifications, please check our Git repository. Thanks for watching, Team Yoda
View full article
Milestone 4 - "Each recipe must be available for the user via a set of Wi-Fi commands. These commands will trigger the machine into mixing the right drinks for that user." Conexiunea dintre tableta android si udoo a fost realizata prin sockets. Pentru demonstratie a fost aleasa o "bautura" care continea toate cele 4 ingrediente disponibile la cele 4 pompe cu un timp de 9,5 secunde fiecare echivalentul a 50 ml. 
View full article
Aplicatia administrativa a bazei de date. Design-ul este inca primar deoarece sunt singur in echipa si nu am apucat sa fac si design-ul dar core-ul merge. Pentru cine vrea sa vada cum merge cu mana lui: Adresa: catalin.etrandafir.ro Cont administrator: username - admin parola - admin Daca se buguieste puteti sa puneti un comentariu :smileygrin:
View full article