ls1046ardb NAND and CPLD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046ardb NAND and CPLD

ソリューションへジャンプ
1,513件の閲覧回数
renaud
Contributor IV

On the LS1046ARDB, is the CPLD in the way of the NAND? I see some signal for the NAND go through the CPLD.

Is there any registers to be programmed in the CPLD to enable access to the NAND?

I am having difficulties accessing the NAND on my boot loader.

 

Cheers,

Renaud

0 件の賞賛
返信
1 解決策
1,508件の閲覧回数
ufedor
NXP Employee
NXP Employee

There are only two signals go through CPLD: NAND_CS_B and NAND_RB_B and they are statically assigned to ifc_cs0 and ifc_rb0.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,509件の閲覧回数
ufedor
NXP Employee
NXP Employee

There are only two signals go through CPLD: NAND_CS_B and NAND_RB_B and they are statically assigned to ifc_cs0 and ifc_rb0.

0 件の賞賛
返信