ls1046a RCW source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046a RCW source

Jump to solution
2,255 Views
Daves_Garage
Contributor IV

I'm confused about the valid location for the RCW in the LS1046A.

In LS1046A Reference Manual, Rev. 3, 08/2021, page 208, it states:

"NOTE: LS1046A do not support NAND flash as RCW source."

but on page 209, step 10, it states:

"If the IFC's NAND Flash interface is configured as the RCW source, the reset block
instructs the IFC to load a boot block from Flash into the internal buffer RAM of the
IFC."

I'm confused reading this, and could use some explanation.

0 Kudos
Reply
1 Solution
2,223 Views
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

View solution in original post

0 Kudos
Reply
1 Reply
2,224 Views
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

0 Kudos
Reply