ls1046a RCW source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ls1046a RCW source

跳至解决方案
2,248 次查看
Daves_Garage
Contributor IV

I'm confused about the valid location for the RCW in the LS1046A.

In LS1046A Reference Manual, Rev. 3, 08/2021, page 208, it states:

"NOTE: LS1046A do not support NAND flash as RCW source."

but on page 209, step 10, it states:

"If the IFC's NAND Flash interface is configured as the RCW source, the reset block
instructs the IFC to load a boot block from Flash into the internal buffer RAM of the
IFC."

I'm confused reading this, and could use some explanation.

0 项奖励
回复
1 解答
2,216 次查看
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,217 次查看
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

0 项奖励
回复