ls1046a RCW source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,242件の閲覧回数
Daves_Garage
Contributor IV

I'm confused about the valid location for the RCW in the LS1046A.

In LS1046A Reference Manual, Rev. 3, 08/2021, page 208, it states:

"NOTE: LS1046A do not support NAND flash as RCW source."

but on page 209, step 10, it states:

"If the IFC's NAND Flash interface is configured as the RCW source, the reset block
instructs the IFC to load a boot block from Flash into the internal buffer RAM of the
IFC."

I'm confused reading this, and could use some explanation.

0 件の賞賛
返信
1 解決策
2,210件の閲覧回数
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,211件の閲覧回数
Daves_Garage
Contributor IV

The LS1046A does not support NAND flash as an RCW source.

0 件の賞賛
返信