ls1028ard secure boot failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1028ard secure boot failed

5,146件の閲覧回数
540915622
Contributor III

The lsdk version is :flexbuild_lsdk2004_update_290520

I use this  command "flex-builder -i mkfw -m ls1028ardb -b xspi -s" and "flex-builder -i mkfw -m ls1028ardb -b sd -s" to generate SD card and xspi boot image .

Then use "flex-installer -f /mnt/firmware_ls1028ardb_uboot_xspiboot_secure.img -d /dev/mtdblock0" and "flex-installer -f /mnt/firmware_ls1028ardb_uboot_sdboot_secure.img -d /dev/mmcblk0" to deploy.

When I set to the corresponding startup mode, I can’t start, and there is no output from the serial port. 

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

5,057件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior TAP with CCS is used in the prototype design stage. In the production stage, you could write OTPMK and SRK keys to shadow registers under u-boot and blow them to fuse arrays permanently.

0 件の賞賛
返信

5,057件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "6.1.5 Procedure to run secure boot" in document "Layerscape Software Development Kit User Guide 20.04" downloaded from" Layerscape SDK | NXP 

0 件の賞賛
返信

5,058件の閲覧回数
540915622
Contributor III

You can send me a SD card secure boot image ?

0 件の賞賛
返信

5,058件の閲覧回数
540915622
Contributor III

I refer to this document, there is no safe boot procedure for ls1028 in the document.

pastedImage_1.png

0 件の賞賛
返信

5,057件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

To below OTPMK, put jumper on J28 (TA_PROG_SFP) to supply 1.8 V to PROG_SFP

0 件の賞賛
返信

5,057件の閲覧回数
540915622
Contributor III

The following operations must be configured using codewarror and CW TAP?

Is there no other configuration method? Is it too troublesome to operate in a production environment?

0 件の賞賛
返信