ls1028ard secure boot failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1028ard secure boot failed

5,221 次查看
540915622
Contributor III

The lsdk version is :flexbuild_lsdk2004_update_290520

I use this  command "flex-builder -i mkfw -m ls1028ardb -b xspi -s" and "flex-builder -i mkfw -m ls1028ardb -b sd -s" to generate SD card and xspi boot image .

Then use "flex-installer -f /mnt/firmware_ls1028ardb_uboot_xspiboot_secure.img -d /dev/mtdblock0" and "flex-installer -f /mnt/firmware_ls1028ardb_uboot_sdboot_secure.img -d /dev/mmcblk0" to deploy.

When I set to the corresponding startup mode, I can’t start, and there is no output from the serial port. 

标签 (2)
0 项奖励
回复
6 回复数

5,132 次查看
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior TAP with CCS is used in the prototype design stage. In the production stage, you could write OTPMK and SRK keys to shadow registers under u-boot and blow them to fuse arrays permanently.

0 项奖励
回复

5,132 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "6.1.5 Procedure to run secure boot" in document "Layerscape Software Development Kit User Guide 20.04" downloaded from" Layerscape SDK | NXP 

0 项奖励
回复

5,133 次查看
540915622
Contributor III

You can send me a SD card secure boot image ?

0 项奖励
回复

5,133 次查看
540915622
Contributor III

I refer to this document, there is no safe boot procedure for ls1028 in the document.

pastedImage_1.png

0 项奖励
回复

5,132 次查看
yipingwang
NXP TechSupport
NXP TechSupport

To below OTPMK, put jumper on J28 (TA_PROG_SFP) to supply 1.8 V to PROG_SFP

0 项奖励
回复

5,132 次查看
540915622
Contributor III

The following operations must be configured using codewarror and CW TAP?

Is there no other configuration method? Is it too troublesome to operate in a production environment?

0 项奖励
回复