cpu hotplug does not work on ls1028a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cpu hotplug does not work on ls1028a

ソリューションへジャンプ
4,887件の閲覧回数
zumengchen
Contributor III

Hi experts,

Could you please help me to confirm if this is this hardware issue as shown in P.S., thanks

I believe you can tell it is your kernel from the output of `uname`, I think the same issue should be seen in both your 0.2 and 0.3 SDK.

Cheers,

Zumeng

root@ls1028a:/sys/devices/system/cpu/cpu1# uname -a
Linux ls1028a 4.14.47-51091-g985a1f51c31c #2 SMP PREEMPT Wed Dec 19 11:41:09 IST 2018 aarch64 GNU/Linux
root@ls1028a:/sys/devices/system/cpu/cpu1#

root@ls1028a:/sys/devices/system/cpu/cpu1# ls -l
total 0
drwxr-xr-x 6 root root 0 May 8 11:52 cache
-rw-r--r-- 1 root root 4096 May 8 11:52 cpu_capacity
lrwxrwxrwx 1 root root 0 May 8 11:52 cpufreq -> ../cpufreq/policy0
drwxr-xr-x 5 root root 0 May 8 11:52 cpuidle
-r-------- 1 root root 4096 May 8 11:52 crash_notes
-r-------- 1 root root 4096 May 8 11:52 crash_notes_size
drwxr-xr-x 2 root root 0 May 8 11:52 hotplug
lrwxrwxrwx 1 root root 0 May 8 11:52 node0 -> ../../node/node0
lrwxrwxrwx 1 root root 0 May 8 11:52 of_node -> ../../../../firmware/devicetree/base/cpus/cpu@1
-rw-r--r-- 1 root root 4096 May 8 11:52 online
drwxr-xr-x 2 root root 0 May 8 11:52 power
drwxr-xr-x 3 root root 0 May 8 11:52 regs
lrwxrwxrwx 1 root root 0 May 8 11:44 subsystem -> ../../../../bus/cpu
drwxr-xr-x 2 root root 0 May 8 11:52 topology
-rw-r--r-- 1 root root 4096 May 8 11:44 uevent
root@ls1028a:/sys/devices/system/cpu/cpu1# echo 0 > online
[ 495.454219] psci: unable to power off CPU1 (-95)
[ 495.454221] CPU1: shutdown
[ 495.461561] ------------[ cut here ]------------
[ 495.466188] kernel BUG at arch/arm64/kernel/smp.c:394!
[ 495.471341] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP
[ 495.473977] psci: Retrying again to check for CPU kill
[ 495.481990] Modules linked in:
[ 495.485052] CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.14.47-51091-g985a1f51c31c #2
[ 495.492820] Hardware name: LS1028A RDB Board (DT)
[ 495.493983] psci: Retrying again to check for CPU kill
[ 495.502684] task: ffff80207b376180 task.stack: ffff000009788000
[ 495.508628] PC is at cpu_die+0x40/0x48
[ 495.512385] LR is at cpu_die+0x40/0x48
[ 495.513973] psci: Retrying again to check for CPU kill
[ 495.521289] pc : [<ffff000008090460>] lr : [<ffff000008090460>] pstate: 000001c5
[ 495.528707] sp : ffff00000978bf40
[ 495.532026] x29: ffff00000978bf40 x28: ffff000000000001
[ 495.533974] psci: Retrying again to check for CPU kill
[ 495.542503] x27: 0000000000000002 x26: 0000000000000002
[ 495.547832] x25: ffff000000000001 x24: 0000000000000000
[ 495.553160] x23: ffff00000a07bbc0 x22: ffff000009468158
[ 495.553974] psci: Retrying again to check for CPU kill
[ 495.563637] x21: ffff00000947a000 x20: ffff00000947a970
[ 495.568964] x19: 0000000000000001 x18: 0000000000000010
[ 495.573985] psci: Retrying again to check for CPU kill
[ 495.579440] x17: 0000ffffaae8855c x16: ffff00000820eb00
[ 495.584768] x15: 0000000000000006 x14: ffff0000896043af
[ 495.590095] x13: ffff0000096043bd x12: ffff000009495d10
[ 495.593975] psci: Retrying again to check for CPU kill
[ 495.600571] x11: ffff00000978bc20 x10: 0000000005f5e0ff
[ 495.605898] x9 : 00000000ffffffd0 x8 : 000000000006ee4d
[ 495.611225] x7 : ffff00000869d4f8 x6 : 0000000000000218
[ 495.613972] psci: Retrying again to check for CPU kill
[ 495.621702] x5 : 0000000000000000 x4 : 0000000000000000
[ 495.627029] x3 : 0000000000000000 x2 : ffff80207b376180
[ 495.632356] x1 : ffff80207b376180 x0 : 0000000000000024
[ 495.633976] psci: Retrying again to check for CPU kill
[ 495.642834] Process swapper/1 (pid: 0, stack limit = 0xffff000009788000)
[ 495.649554] Call trace:
[ 495.652002] Exception stack(0xffff00000978be00 to 0xffff00000978bf40)
[ 495.653977] psci: Retrying again to check for CPU kill
[ 495.653980] psci: CPU1 may not have shut down cleanly (AFFINITY_INFO reports 0)
[ 495.653982] CPU1 may not have shut down cleanly: -110
[ 495.675999] be00: 0000000000000024 ffff80207b376180 ffff80207b376180 0000000000000000
[ 495.683853] be20: 0000000000000000 0000000000000000 0000000000000218 ffff00000869d4f8
[ 495.691708] be40: 000000000006ee4d 00000000ffffffd0 0000000005f5e0ff ffff00000978bc20
root@ls1028a:/sy[ 495.699562] be60: ffff000009495d10 ffff0000096043bd ffff0000896043af 0000000000000006
[ 495.708807] be80: ffff00000820eb00 0000ffffaae8855c 0000000000000010 0000000000000001
[ 495.716662] bea0: ffff00000947a970 ffff00000947a000 ffff000009468158 ffff00000a07bbc0
s/devices/system[ 495.724516] bec0: 0000000000000000 ffff000000000001 0000000000000002 0000000000000002
/cpu/cpu1# [ 495.733761] bee0: ffff000000000001 ffff00000978bf40 ffff000008090460 ffff00000978bf40
[ 495.742573] bf00: ffff000008090460 00000000000001c5 0000000000000000 0000000000000000
[ 495.750427] bf20: ffffffffffffffff ffff000008090460 ffff00000978bf40 ffff000008090460
[ 495.758284] [<ffff000008090460>] cpu_die+0x40/0x48
[ 495.763089] [<ffff000008085514>] arch_cpu_idle_dead+0xc/0x18
[ 495.768767] [<ffff00000810b000>] do_idle+0x128/0x1d8
[ 495.773745] [<ffff00000810b244>] cpu_startup_entry+0x24/0x28
[ 495.779420] [<ffff0000080902e8>] secondary_start_kernel+0x110/0x120
[ 495.785706] Code: 2a1303e0 f8735821 f9401821 d63f0020 (d4210000)
[ 495.791822] ---[ end trace 5cdaa85e26845d44 ]---
[ 495.796451] Kernel panic - not syncing: Attempted to kill the idle task!
[ 495.803172] Kernel Offset: disabled
[ 495.806667] CPU features: 0x1802008
[ 495.810161] Memory Limit: none
[ 495.813221] ---[ end Kernel panic - not syncing: Attempted to kill the idle task!

root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1# cat /proc/cpuinfo
processor : 0
BogoMIPS : 50.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3

root@ls1028a:/sys/devices/system/cpu/cpu1# echo 1 > online
[ 503.366239] psci: failed to boot CPU1 (-22)
[ 503.370444] CPU1: failed to boot: -22

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
[ 503.380077] CPU1: failed in unknown state : 0x0
ls1028a kernel: [ 495.471341] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.785706] Code: 2a1303e0 f8735821 f9401821 d63f0020 (d4210000)

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.642834] Process swapper/1 (pid: 0, stack limit = 0xffff000009788000)

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.796451] Kernel panic - not syncing: Attempted to kill the idle task!

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.806667] CPU features: 0x1802008

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.803172] Kernel Offset: disabled

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.810161] Memory Limit: none

Message from syslogd@ls1028a at Wed May 8 11:53:10 2019 ...
ls1028a kernel: [ 495.813221] ---[ end Kernel panic - not syncing: Attempted to kill the idle task!
-sh: echo: write error: Invalid argument
root@ls1028a:/sys/devices/system/cpu/cpu1#
root@ls1028a:/sys/devices/system/cpu/cpu1# cat /proc/cpuinfo
processor : 0
BogoMIPS : 50.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3

root@ls1028a:/sys/devices/system/cpu/cpu1# uname -a
Linux ls1028a 4.14.47-51091-g985a1f51c31c #2 SMP PREEMPT Wed Dec 19 11:41:09 IST 2018 aarch64 GNU/Linux
root@ls1028a:/sys/devices/system/cpu/cpu1#

タグ(1)
0 件の賞賛
返信
1 解決策
4,701件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached console log, I am using BSP 0.3 pre-built image lsdk_linux_arm64_LS_tiny.itb.

Thanks,

Yiping

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,701件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello zumeng chen,

I checked ls1028a-bsp0.3 image lsdk_linux_arm64_LS_tiny.itb on LS1028ARDB, it seems that CPU hotplug feature can work normally, please refer to my following log on LS1028ARDB.

root@TinyDistro:~# ls /sys/devices/system/cpu/cpu1/
cache             cpuidle           hotplug           online            subsystem
cpu_capacity      crash_notes       node0             power             topology
cpufreq           crash_notes_size  of_node           regs              uevent
root@TinyDistro:~# cd /sys/devices/system/cpu/cpu1/

root@TinyDistro:/sys/devices/system/cpu/cpu1# echo 0 > online
[  134.082783] CPU1: shutdown
[  134.085500] psci: CPU1 killed.
root@TinyDistro:/sys/devices/system/cpu/cpu1# cat /proc/cpuinfo

processor       : 0
BogoMIPS        : 50.00
Features        : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant     : 0x0
CPU part        : 0xd08
CPU revision    : 3

root@TinyDistro:/sys/devices/system/cpu/cpu1# cat /proc/cpuinfo
processor       : 0
BogoMIPS        : 50.00
Features        : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant     : 0x0
CPU part        : 0xd08
CPU revision    : 3

root@TinyDistro:/sys/devices/system/cpu/cpu1# echo 1 > online
[  207.958845] Detected PIPT I-cache on CPU1
[  207.962887] GICv3: CPU1: found redistributor 1 region 0:0x0000000006060000
[  207.969813] CPU1: Booted secondary processor [410fd083]
root@TinyDistro:/sys/devices/system/cpu/cpu1# cat /proc/cpuinfo
processor       : 0
BogoMIPS        : 50.00
Features        : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant     : 0x0
CPU part        : 0xd08
CPU revision    : 3

processor       : 1
BogoMIPS        : 50.00
Features        : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant     : 0x0
CPU part        : 0xd08
CPU revision    : 3

root@TinyDistro:/sys/devices/system/cpu/cpu1#


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,701件の閲覧回数
zumengchen
Contributor III

Hi Yiping, 

Can you please paste me the following information, thanks a lot

   1 ) Your u-boot welcome information

   2 ) Your  first kernel commit log

   3 ) Your hardware version information, including board and SoC

Cheers,

Zumeng

0 件の賞賛
返信
4,702件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached console log, I am using BSP 0.3 pre-built image lsdk_linux_arm64_LS_tiny.itb.

Thanks,

Yiping

0 件の賞賛
返信