System Clock Frequency for LS1028ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System Clock Frequency for LS1028ardb

Jump to solution
1,798 Views
SoccerMom
Contributor II

I am using the LS1028ARDB (Armv8) board. The RCW setting for System Clock is 0x258 which is 100 MHz. I am using the arm generic timer to calculate execution time. The cntfrq_el0 reads a zero. I am running the bare metal configuration. To check the the counter i read the cntpct_el0. But to calculate the time I need the actual frequency. Arm says that for Armv8 the system clock is usually 1 to 50 Mhz. I dont know what value of system clock should I be using?

0 Kudos
Reply
1 Solution
1,779 Views
yipingwang
NXP TechSupport
NXP TechSupport

It is 25MHz for LS1028A.

View solution in original post

0 Kudos
Reply
1 Reply
1,780 Views
yipingwang
NXP TechSupport
NXP TechSupport

It is 25MHz for LS1028A.

0 Kudos
Reply