System Clock Frequency for LS1028ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System Clock Frequency for LS1028ardb

ソリューションへジャンプ
1,789件の閲覧回数
SoccerMom
Contributor II

I am using the LS1028ARDB (Armv8) board. The RCW setting for System Clock is 0x258 which is 100 MHz. I am using the arm generic timer to calculate execution time. The cntfrq_el0 reads a zero. I am running the bare metal configuration. To check the the counter i read the cntpct_el0. But to calculate the time I need the actual frequency. Arm says that for Armv8 the system clock is usually 1 to 50 Mhz. I dont know what value of system clock should I be using?

0 件の賞賛
返信
1 解決策
1,770件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It is 25MHz for LS1028A.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,771件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It is 25MHz for LS1028A.

0 件の賞賛
返信