Question regarding device tree definition of ls1021a.dtsi and .dts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question regarding device tree definition of ls1021a.dtsi and .dts

1,096 Views
jiye
Contributor V

Hi,

I understand that the .dtsi is from SoC chip level and .dts is from board level respectively.

I have a question when comes to this ls1021a.dtsi

pastedImage_1.png

(1)Why there is a gpio3 there at the node section, what does that use for?

pastedImage_2.png

(2)And why sysclk doesn't have a cell for address register because sysclk isn't a memory I/O device?

(3) Also the status section 

pastedImage_2.png

can this be inside of the .dtsi as well, I thought this can only be inside of the .dts file only to disable or enable the node.

Labels (2)
0 Kudos
Reply
1 Reply

1,045 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. It is used to define GPIO module.

pastedImage_1.png

2. Yes, sysclk isn't a memory I/O device.

3. Status can be used inside of the .dtsi.

0 Kudos
Reply