QCVS validation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS validation

Jump to solution
3,899 Views
muaxi8
Contributor V

Platform: LX2160A customized board card。and my ddr4 is discrete type.

I did the validation with QCVS, then what should I do to use the calibrated value.

muaxi8_0-1626241692981.png

 

0 Kudos
Reply
1 Solution
3,868 Views
yipingwang
NXP TechSupport
NXP TechSupport

This should be the code for the slave core, entering into sleep mode. Please attach to the master core to check the problem code.

View solution in original post

0 Kudos
Reply
6 Replies
3,890 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "1.1.1.2 Configure DDR controller" in the attached QCVS DDRv user guide.

After creating a QCVS DDR project for Discreate DRAM with the default parameters, please fill "Properties" panel according to your DDR Datasheet.

0 Kudos
Reply
3,887 Views
muaxi8
Contributor V

hi yipingwnag:

how to use codewarrior to debug uboot ? my pbl It's already ok, but my uboot can  not start up.

0 Kudos
Reply
3,876 Views
muaxi8
Contributor V

hello.

when i debugging uboot with codeworrior, my uboot  is wrong here: cbz x0, slave_cpu.

What does the mean of "slave_cpu",  What cause the wrong here?

thanks.

muaxi8_0-1626351894105.png

 

0 Kudos
Reply
3,855 Views
muaxi8
Contributor V

 

 

 

 

0 Kudos
Reply
3,869 Views
yipingwang
NXP TechSupport
NXP TechSupport

This should be the code for the slave core, entering into sleep mode. Please attach to the master core to check the problem code.

0 Kudos
Reply