PHY handshake timeout..., ddr_dsr2 = 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PHY handshake timeout..., ddr_dsr2 = 0

11,259 次查看
muaxi8
Contributor V

platform: LX2080a

ddr4:  MT40A512M16JY ,8Gb, x16 width

I program the bl2_flexspi_nor.pbl,  fip_uboot.bin, fip_ddr_all.bin  on the specific address。

The following print appears when  my board is power on。What causes DDR PHY to fail ? 

i  have Defined macro “CONFIG_STATIC_DDR” in plat/nxp/<SOC>/<BOARD>/plafform_def.h to enable discrete DDR timings.

NOTICE:  BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE:  BL2: Built : 18:47:53, May  7 2021
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
ERROR:   Found training error(s): 0x100
ERROR:   Error: Waiting for D_INIT timeout.
ERROR:   Writing DDR register(s) failed
ERROR:   Programing DDRC error
ERROR:   DDR init failed.
NOTICE:  Incorrect DRAM0 size is defined in platform_def.h

 

0 项奖励
回复
17 回复数

11,208 次查看
muaxi8
Contributor V
  1. 补充:
    芯片型号:LX2080XE72232B

  2. ddr4: MT40A512M16JY-083EIT
0 项奖励
回复

11,165 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached QCVS DDRv user manual. 

Please configure "Properties" panel according to your DDR data sheet, then generate the initial DDR controller configuration parameter. Then you need to connect DDRv tool to your target board to optimize and validate these DDR configuration parameters.

0 项奖励
回复

11,166 次查看
muaxi8
Contributor V

yes, i connected DDRv tool to my target board,and "start validation", but it is Execution failed and will not proceed。I tried  several times but  still failed.

muaxi8_0-1621588047058.png

 

0 项奖励
回复

11,119 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please open CCS(CodeWarrior Connection Server) console, type "log v" command, then connect to the target board again? The low level CCS log will be printed. Please capture the CCS log and attach it to this thread.

0 项奖励
回复

11,102 次查看
muaxi8
Contributor V

The attachment is the log, but the previous contents seem to have been flushed out..

There was a mistake at the beginning:

muaxi8_0-1621911773201.png

 

0 项奖励
回复

11,093 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "DDR Bring up issue"(page 2)  and "DDR Bring up HW checklist" (page 4)  sections in the attached document.

0 项奖励
回复

11,071 次查看
xmj
Contributor I

Hi yipingwang, 

Is this documentation also for LX2160A? 

Thanks

0 项奖励
回复

11,036 次查看
yipingwang
NXP TechSupport
NXP TechSupport

This document is also for LX2160A.

0 项奖励
回复

11,122 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please provide Error capture registers values?

0 项奖励
回复

11,104 次查看
muaxi8
Contributor V

 this is the  Error capture registers values...there valuse are all 0x0

muaxi8_0-1621912246038.png

 

muaxi8_1-1621912272509.png

 

muaxi8_2-1621912320803.png

 

muaxi8_3-1621912337942.png

 

 

0 项奖励
回复

11,240 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You need to modify "const struct ddr_cfg_regs static_1600" in atf/plat/nxp/<SOC>/<BOARD>/ddr_init.c according to the DDR on your target board.

You could use QCVS DDRv tool to assist you to calculate DDR controller configuration parameters and optimize them.

0 项奖励
回复

11,231 次查看
muaxi8
Contributor V

 

AS the following figure。there is a Lead-in paramter , don't know how to fill in this parameter, How do I get this parameter?

muaxi8_0-1620976555169.png

Thank you for your reply

0 项奖励
回复

11,210 次查看
yipingwang
NXP TechSupport
NXP TechSupport

No need to fill this parameter.

0 项奖励
回复

11,178 次查看
muaxi8
Contributor V

muaxi8_0-1621501163204.png

Does the DQ mapping need to be configured? my dram type is discrete...

0 项奖励
回复

11,183 次查看
muaxi8
Contributor V

help me please

0 项奖励
回复

11,202 次查看
muaxi8
Contributor V

  I configured the above values based on the hardware's CLK To DQS parameters, and then generated the code in CodeWarrior, i Copy the static_1600 to my source code

 

 

const struct ddr_cfg_regs static_1600 = {
        .cs[0].config = 0x80010412,
        .cs[0].bnds = 0xFF,
        .sdram_cfg[0] = 0x65240000,
        .sdram_cfg[1] = 0x00401030,
        .timing_cfg[0] = 0x8055000C,
        .timing_cfg[1] = 0x0A0E0C42,
        .timing_cfg[2] = 0x0048D11C,
        .timing_cfg[3] = 0x11511000,
        .timing_cfg[4] = 0x01,
        .timing_cfg[5] = 0x05401400,
        .timing_cfg[7] = 0x23340000,
        .timing_cfg[8] = 0x07116600,
        .sdram_mode[0] = 0x01010234,
        .sdram_mode[9] = 0x0701,
        .sdram_mode[8] = 0x00,
        .sdram_mode[2] = 0x00,
        .sdram_mode[10] = 0x04000000,
        .sdram_mode[11] = 0x00,
        .sdram_mode[4] = 0x00,
        .sdram_mode[12] = 0x00,
        .sdram_mode[13] = 0x00,
        .sdram_mode[6] = 0x00,
        .sdram_mode[14] = 0x00,
        .sdram_mode[15] = 0x00,
        .interval = 0x18600618,
        .zq_cntl = 0x8A090705,
        .wrlvl_cntl[0] = 0x00,
        .wrlvl_cntl[1] = 0x00,
        .wrlvl_cntl[2] = 0x00,
        .debug[28] = 0x01080F70
};

 

 

 

After compiling with the flex-builder -c atf -m lx2160ardb_rev2 -b xspi command, bl2_flexspi_nor.pbl and fip_uboot.bin,programmed it to the  Flash, but it still prompts the 2D Training .(I turned on the Debug switch).Debugging several days, all the time not to the main point

 

 

muaxi8_0-1621335185653.png

 The following is the log information, looking forward to your reply...

 

NOTICE:  BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE:  BL2: Built : 16:15:55, May 18 2021
platform clock 800000000
DDR PLL1 1600000000
DDR PLL2 1600000000
frequency = 800MHz
Vref_phy = 75 percent
Initializing input adv data structure
mr[0] = 0x234
mr[1] = 0x101
mr[2] = 0x0
mr[3] = 0x0
mr[4] = 0x0
mr[5] = 0x0
mr[6] = 0x0
input->cs_d0 = 0x3
input->cs_d1 = 0x0
input->mirror = 0x0
PHY ODT impedance = 48 ohm
PHY DQ driver impedance = 28 ohm
PHY Addr driver impedance = 30 ohm
odt[0] = 0x1
odt[1] = 0x0
odt[2] = 0x0
odt[3] = 0x0
Initializing message block
msg_blk->dram_type = 0x2
msg_blk->sequence_ctrl = 0x31f
msg_blk->phy_cfg = 0x0
msg_blk->x16present = 0x3
msg_blk->dramfreq = 0x640
msg_blk->pll_bypass_en = 0x0
msg_blk->dfi_freq_ratio = 0x2
msg_blk->phy_odt_impedance = 0x0
msg_blk->phy_drv_impedance = 0x0
msg_blk->bpznres_val = 0x0
msg_blk->enabled_dqs = 0x48
msg_blk->acsm_odt_ctrl0 = 0x1
msg_blk->acsm_odt_ctrl1 = 0x0
msg_blk->acsm_odt_ctrl2 = 0x0
msg_blk->acsm_odt_ctrl3 = 0x0
rx2d_train_opt 0, tx2d_train_opt 0
Initialize PHY 0 config
pll_ctrl2 = 0xb
SOC_SI_REV = 2
dll_lck_param = 0x212
dll_gain_ctl = 0x61
acx4_anib_Dis 0x0
Load 1D firmware
Loaded Imaged id 32 of size 6bd0 at address 18003000
Loaded Imaged id 34 of size 6d0 at address 18003000
Execute firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of fine write leveling
1D Training completed
Error - Invalid cs_in_use value 0
CDD rrmax 3 wwmax 4 rwmax 2 wrmax 0
Load 2D firmware
Loaded Imaged id 33 of size 694c at address 18003000
Loaded Imaged id 35 of size 5bc at address 18003000
Execute 2D firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of initialization
End of initialization
End of initialization
2D Training failure
ERROR:   Execution FW failed (err -5)
Program controller registers
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
total size 4 GB
Need to wait up to 1320 ms
ERROR:   Found training error(s): 0x100
ERROR:   Error: Waiting for D_INIT timeout.
ERROR:   Writing DDR register(s) failed
ERROR:   Programing DDRC error
ERROR:   DDR init failed.
NOTICE:  Incorrect DRAM0 size is defined in platform_def.h -5

 

 

 

 

 

 

 

0 项奖励
回复

11,170 次查看
xmj
Contributor I

I am working on the same issue......

0 项奖励
回复