About the USB controller of LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the USB controller of LS1046A

Jump to solution
2,449 Views
okamotosatoshi
Contributor IV

Hi There,

 

I want to check how to use the USB controller of LS1046A.

There is a difference between the contents of the reference board and the application note.

Please tell me the correct unused processing the following conditions.

 

[Conditions]

 ・USB1 works with USB2.0.

 ・USB2 / 3 is unused.

 

【Check】

1.Does USB [2/3] _VBUS need a 5V power supply?

2.Is the USB [2/3] _ID 1kΩ connection correct?

3.Does USB [1] _RESREF require 200Ω?

4.Does USB [2/3] _RESREF require 200Ω?

 

Best regards

- satoshi

0 Kudos
Reply
1 Solution
2,443 Views
ufedor
NXP Employee
NXP Employee

1) Could be left unconnected.

2) Yes.

3) Yes.

4) Could be left unconnected.

View solution in original post

0 Kudos
Reply
2 Replies
2,444 Views
ufedor
NXP Employee
NXP Employee

1) Could be left unconnected.

2) Yes.

3) Yes.

4) Could be left unconnected.

0 Kudos
Reply
2,438 Views
okamotosatoshi
Contributor IV

Hi ufedor

 

Thank you for your answer!

I will do the terminal processing of the advice.

 

Best regards
- satoshi

0 Kudos
Reply